This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Schematic and Layout Tools

Other Parts Discussed in Thread: UCC28710

Hi,

can I know which tool I have to use to read .sch and .pcb files released with PMP4480 Ref.Design.

Regards,

Valerio

  • Hi

    The is a link to a viewer on the web page, other than that the files are either PADs or Altium.

    Regards

    Peter
  • Thanks,

    I checked design and I verify that the Transformer I ordered according to suggested BOM is for 5V@1A instead of 12V@1A I expected. Could I set the board using this transformer for 12V@1A not allowing 85VAC as per minimum line voltage but accepting 150-180VAC as per ucc simulation ?

    It will help me not to waste time in remaking the completelly the prototypes. TI ucc28710 tool allow 14:1 and 6,59:1 ratios if minimum voltage level is increased; it is viable ?

    Regards

    Valerio