Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51367 PGOOD Question

Other Parts Discussed in Thread: TPS51367

Hello

I am question about the TPS51367.

It'll be attached documents about the contents.

Thank you.

TPS51367Q.pdf

  • For almost any IC as the input voltage starts to rise from zero, there is no control over the internal functions as there is not enough input voltage for the internal circuitry to work properly. As the input voltage rises to about 0.6 V to 0.8V, some internal PN junctions may become forward biased and allow some voltage to appear at output pins. As the voltage continues to rise up above about 1.2 V, the internal circuitry becomes aware and can control their functions such as PGOOD and force the outputs low or high as required. This is what you are seeing in your diagram.