The application is to drive a string of 3.5V LEDs at 5-10KHz with ~50% duty cycle (On and Off). The drive current need to be adjustable or programmable (I2C bus preferred) from 100mA to 1A (2-300mA if combining outputs).
It requires the controller or driver to be able to switch on and off the LEDs in a few us at full load (100mA to 1A).
I am looking at
1) LM3550, not sure if I can switch on and off the external driver without disstablizing the control loop in torch mode.
2) TPS61196, looks promising. Need resistor to set the current and combine 2-3 outputs to drive one LED string.
3) LM3409, data sheet shows clear fast enough on/off time (page 9).
... ...
Any suggestions or recommendations are appreciated.
F.Z.