This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2002/3C Dual Power Distribution Switch input

Other Parts Discussed in Thread: TPS2043B

Referring to the datasheet (SLVSAX6G) for the TPS20xxC dual channel, current-limited, power-distribution switch, I note that the DRC package has two input pins (IN) whereas all other packages have a single input.  All the functional block diagrams show a single IN pin, so can I assume that the two IN pins on the DRC package are tied together or are they actually two independent channels to OUT1 and OUT2, respectively?  If the IN pins are common, is there a device with two truly independent switchable paths: IN1 --> OUT1 and IN2 --> OUT2?  I have two independent USB channels I wish to perform a hard reset on (independently) by controlling the VBUS connection to the downstream port.  It would be great if it also had the output discharge feature like these devices.  I suspect that I will need to look at using two of the single channel devices in this family (TPS2000/1C).