Hi all,
I'm disty in Japan.
My customer is designing a prototype including the TPS54618Q1 now.
He'd like to change the fsw frequency in his application,
so he is considering a external circuit.
I attached his current circuit plan.
*Cf. attached file TPS54618Q1_extclk.xlsx
*I add the circuit plan2 which I am suggesting to him.
TPS54618Q1_extclk.xlsx
He would like to use the circuit plan1, because it is low cost.
I have two questions.
Question1)
Is the circuit plan1 usable by adjusting capacitor value?
Question2)
Is there any problem about the circuit plan2?
Best regards.
Tsuyoshi Tokumoto