We plan to use BQ24650 as a charger for charging 12V Lead acid batteries (@ maximum current of 10A) in our system as well as to provide a system rail voltage in our system. The input voltage to BQ24650 will come from a 17V solar panel (Voc= 22v , Vmp=17.5V) . Accordingly the Sense resistor , inductor etc will be sized according to this maximum 10A charging current requirement
We are using BQ24650 because we are interested in using MPPT capability of BQ24650. So as long as solar panel gives enough power output the batteries continue charging at high current ( ~10A) . Of course if the solar panel voltage drops due to illumination conditions accordingly the charge current into the batteries will be reduced. This is fine with us.
However we have one more requirement of overriding the maximum charging current dynamically. Basically if the ambient temperature inside our equipment becomes high we would like to reduce dynamically the charging current to lower values , say 2A. We want to do this so that the heat dissipation inside our equipment can be reduced. (Because obviously heat dissipation inside equipment will be more when the BQ24650 is charging batteries at 10A versus when BQ24650 is charging batteries at 2A.)
So i have following three questions regarding this
1. From the datasheet of BQ24650,i did not find any way of dynamically changing the charging current, however i was just thinking that is it possible to have some external circuit which can force the voltage on MPPSET to lower than 1.2V ( but greater than 175mv) to reduce the charging current? . Can any such external circuit be suggested by TI ?
2. This question is on a seperate note. What happens when i provide the Vin input to BQ24650 from a DC source of following vales
a) say 13-13.5V V - So of course i , know that from this low voltage adequate voltage for charging lead acid battery can not be generated , hence batteries will not get charged - but question is that whether BQ24650 will try to charge the batteries still or not ?
b) say 24V - this will force the MPPSET pin voltage to be much greater than 1.2V - so does this condition make BQ24650 assume that there is some fault condition and stop charging or will it continue the charging at full current assuming that more than enough power is available for charging