This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Suitable DC-DC Buck converter for coin cell battery with Storage capacitor

Hi,

We are looking for a DC-DC buck converter which will be used with a coin cell (3.6V down to about 2 Volts). The output voltage will be about 2.1 V.

In order to increase battery life, the maximum current drain from the battery should be around 2 mA for short periods only (some seconds). Coin cell battery capacity is reduced if exposed to high pulse currents.

During these seconds, the output storage capacitor should store enough energy to supply up to 20 to 40 mA for a short duration, typically 10 to 30 ms or thereabout. This ensures that the "high" pulse currents is not drawn from the battery itself.

I have found TS3310 from another manufacturer which have this capability. However, it is a boost converter. So, does TI have any DCDC converter which is designed to meet the criterion mentioned?

Regards,

HC