Page 33 of the data sheet for the TPS737xx shows an example land pattern for the DRB package. The center pad's copper and stencil features are shown, but I don't see any details about the solder mask for the center pad. Should there be a strip of solder mask between the large center part and the four pads on the ends?
I have used this part before and I have never seen any solder on the outer edge of the part for the 4 ground pads like it does for the main 8 pads. I did not include a solder mask strip to separate the middle from the outer pads. It appears to me that the large center part is thieving the solder away from the 4 small ground pads. It seems a narrow strip of solder mask would prevent that from happening.
The narrow strip I am proposing is kind of "solder mask defined", but I don't think it would affect the orientation of the part during reflow. Every other copper feature would be non solder mask defined.
Thanks and regards,
Greg