This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24250 is giving continuous "no battery connected error"

Other Parts Discussed in Thread: BQ24250

I have a BQ24250 with 4.99V in, and a single cell connected.  It is being driven in I2C mode at 100Khz.

Single cell is at 3.65V.

EN1 and EN2 are at GND

536ohm resistor on ILIM

I think this should be charging at 500mA, but I keep getting "no battery connected faults"  Suggestions?

FYI.  Here are the register contents:

Charger Registers:
0 0x38
1 0x8C
2 0x8C
3 0x01
4 0x02
5 0xA8
6 0xE0