Hi,
I am designing a Boost converter based on the LM5175. The design specs are 10-14 VIN and 24VOUT / 6A.
I think efficiency is good (more than 90%) in loading but we have excessive current draw (150mA) at no load and LM5175 body is hot. We suspected to Mosfet rise time and full time, so we tested two type different mosfets “FDS86540” and “BSZ042N06NS” and the results were similar. Is this warming and no load current usual?
Best Regards,
Davari