Hi gents,
I would like to use the TPS63000 to provide a 3V DC from either 2 AA battery rechargeable or 1 Li-ion Cell, so input voltage range goes from 1.8V to 4.2V.
I need an average current of 400mA, but the TPS63000 is switching off when voltage drops bellow 2.3V, could you explain how can i determine the minimum input voltage for my 400mA current output? and what is the maximum current when the input is 1.8V?
Thanks for your help.
Bruno