Hi,
We wants to know how we can decrease the minimum Vin (voltage)? On wich component can we “play” to test a Vin under 110mV?
Second question, on the EVM card the cold start is at 330mv and after we can decrease the Vin voltage to 70mV and the card continue to perform (the DC DC boost function is already OK). We did the same card, but we change some resistors value for UV, OV, OK. But on our card the cold start is good at 330mV but when we decrease the Vin voltage (under 330mV) the BQ25504 stop… So Why the EVM card can start at 330mv and continue to works until 70mV and not our? Which element we have to change or increase?
Thnks for your help!! I become crazy!!!
F. Degremont