I have a very light load of about 600 ohms or 2mA at 3V. I am wondering if I can use the mode pin as an enable line for my circuitry that is connected to the VSUB line. The datasheet says that I need to be able to turn it on and off seperately from the mode pin. Is this a hard requirement and if so, why?