Alex,
During IEC 61000-4-5 testing, an LM5067 failed. There is a small crater just behind 8 in the top of the part. Can you tell me what functions are in that area so I can try to figure out what damaged the part?
Thanks!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Alex,
There are no options to insert rich text formatting. The only buttons are along the top edge of the reply box. I have used "insert file".
Tom