Hi All,
I have question of PWM dimming limit for LED Driver(Based on TPS92511 Application),
1.
The TPS92511 has very fast PWM dimming response time.
For example, if the switching frequency is 500 kHz,
the minimum DIM pulse width is 6µs and the
dimming frequency is 150Hz,
a contrast ratio of more than 1000:1 can be achieved.
can we have use mathematics to explain this relation ??
2.
In fact, duty of TPS92511, can implement PWM dimming freq 30kHz@Vin 13V, Vout 7.2V, Iout 0.5A
D = 7.2/12 approximately 0.55
fast PWM dimming freq 30kHz, Do I need add external shunt FET ??
Thanks all.