We are using BQ24610 charger IC in our design. Design spec is given below:
Adapter Input supply = 28V
Charge current = 3.6A
Charge current threshold set at 0.3A.
Full charge expected is 25.2V as set by VFB resistors.
Issues:
1.Not able to charge a 6-cell Li-ion battery upto 25.2V as given in battery spec.
2.Charge termination LED STAT2 does not glow. Cut-off current observed is 0.2A and maximum voltage charged upto 24.24V.
3.Calculated Charge current I=4.4A after resistor tuning at ISET1, then I am getting Charge current of 3.6A(expected), not with the correct resistor values for 3.6A.
Kindly revert on above issues with the BQ24610 charger IC.