Hello there!
I am replacing a 7805 regulator on production device with an LM2675-5.0, to eliminate the heat sink parts required when the product is drawing 300-500mA in short bursts of perhaps 1 minute, several times per day (typically it is approx 170mA).
My initial layout works, sort of... Perfect voltage output up to about 220mA, using the recommended components from datasheet. Using slightly higher load, >250mA, causes loss of regulation and voltage drop, which recovers in stages as load is reduced, eventually back to +4.97v at around 80mA. Stable again as load increases until about 250ma.
Critical items used are:
47uH coil, Digikey # ASPI-0804T-470M-TCT-ND
Alum caps, Digikey # 493-3938-1-ND & PCE3806CT-ND
Schotk Diode, Digikey # SK32A-TPCT-ND
CB cap Digikey # 399-1167-1-ND
I found that placing a standard scope probe on either of the CB cap pins, that the regulation would work to about 320mA. Using a 100pf cap here did not change anything at all.
Is there a 'typical' error with such a circuit that causes this type of loss of regulation under medium (and higher) load? Perhaps a known/common layout error causes this - or a common mistake in component selection/type?? It is on a 1oz copper 2-sided PCB, so no internal ground plane, etc. I have ordered the EVAL module for further tests, but I really don't know what to look for next. Please assist.
Cheers!