Hi,
I'm building a battery management system using the bq76940. The load will draw ~200 A continuous with over-discharge protection needed at around 400-500 A and short circuit discharge protection needed around 600-700 A.
I'm pretty new to power electronics. Does anyone have any suggestions for the current sensing resistor? Following the suggestions in the documentation, a .3-.5 mOhm resistor would work, but it would need to dissipate 20 W or more under typical loads. I would like to keep to relatively inexpensive surface-mount components if possible. My ideas so far have been to
1) Use 2 or more resistors in parallel for Rsns such that no resistor needs to dissipate more than 10 W or so.
2) Use a hall-effect sensor (such as one from the ACS770xCB series by Allegro) combined with a voltage divider to get the output voltage in the +/- 200mV range.
Would either of these work? Any thoughts/suggestions would be appreciated.
Thanks,
Mark