I'm unsure on how to interpret the EN pin behavior of the TPS709: The data sheet gives a typical shutdown current of 150nA both in overview and in 7.4 Device Function Modes as Ishutdown for low EN, but some lines above, it claims that the EN pin is pulled up (ie. into enabled state) by a 300nA current source, which would mean that if EN is externally put to GND (ie. disabled), the current source delivers its full current to the EN pin.
Assuming there is no internal DC-DC converter that boosts the current, how are the 300nA output achieved?
(Background: I'm planning on having a microprocessor switch off its own power supply in deep sleep states, and if startup takes too long, I need the current source to reliably pull up the GPIO pin that has entered high-Z during brownout).