This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24040 Charger IC schematic

Other Parts Discussed in Thread: BQ24040

Hola,

Below is my schematic of BQ24040 charger IC, do I need to modify it if it has any incorrect?thanks

  • 1. Input bypass capacitor needs to be at least 1uF.

    2. OUT bypass capacitor needs to be at lease 1uF

    3. RPRE-TERM = 2kohm sets the precharge current to 20% of the fast charge current which is 54mA

    4. The TS feature is implemented using an internal 50μA current source to bias the thermistor (designed for use with a 10k NTC β = 3370 (SEMITEC 103AT-2 or Mitsubishi TH05-3H103F) connected from the TS terminal to VSS. Please make sure the thermistor of your choice has the same β for the part to monitor the temperature correctly.

  • Hola Jing,

    This is great and thank you very so much.