Hi,
My customer has question about LM27313.
Could you tell me about questoin?
[Question]
My customer consider to design DCM operation under the following condition.
Vin=3.0V to 4.2V
Vout=17V
Iout=50mA max
L=2.2uH
peak inductor current=650mA at Vin=3.0V
If the device is designed CCM operation, there is concern about maximum Duty limit.
Could you recommend that the device operates in discontinuous mode in this case?
Best Regards,
tateo