I recently joined an R&D group which has a TPS65217A evaluation module (EVM). Yesterday I tried to start it up for the first time. No one has used it for close to two years. I think it may be damaged, but no one who presently works here knows enough about it. Please help me diagnose my problem.
First of all, I'm not using the software yet. I have the USB Interface adapter connected to my computer and the EVM. I have the documentation for the EVM and for the PMIC itself. Page 2 of the EVM manual says: "The EVM will power-up and operate without use of software." That's all I'm trying to do for now. Pages 6 and 7 describe how to configure the jumpers. My setup looks identical to Figure 3 (page 7) except for the fact that I do not have a battery connected. Page 6 says that I should open JP6 if I don't have a battery, so that's what I did.
Figure 1 (page 17) of the TPS65217A data sheet shows the global state diagram. If I am reading it correctly, PGOOD and LDO_PGOOD should both pull high when the ACTIVE state is reached. I see that, I'm getting a steady +3.3V on both lines. However, the white LED drivers should also turn on in ACTIVE state. I'm not seeing any lights. Also, I get no voltage across any of the PMIC output terminals. Shouldn't at least LDO1 be on, and reading 1.0V?
Any advice is appreciated. Thanks!