This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS73033 issue: output is abnormal



Hi,

I'm using TPS73033 device, the input voltage for TPS73033. after solder, we found there are several issues.

1. The output is equal to input 5 V for some devices.

2. There is no output for some devices.

3. The output is 1 V for some devices

4. The output is 2 V for some devices.

 

Is there any guideline to debug these issues?

 

Regards

 

Jin

  • Hi Jin,

    There are a couple of things that should be verified. When you do a visual inspection, do you see any shorts? I would also look for any unintentional leakage paths with flux. These are the most likely causes of so many different voltages.

    Very Respectfully,
    Ryan
  • Hi Ryan,

    I tested the IO pins and didn't find shorts on any IO. But when I configure the device into shut down mode ( EN is configured as GND ),  the current is about 2 mA.

    According to the datasheet, the leakage current is several uA.

    It seems there are some shorts internally.  Has this issue been reported by any user?

     

  • Hi Jin,

    We test our devices before shipping and I am unaware of any similar issues reported before.

    The increased shutdown current is another indicator that there are unintentional leakage paths or shorts on the board.

    Very Respectfully,
    Ryan