Hello-
We had designed in the LM4051 into our boards but then noticed that this part has a maximum reflow temperature of 220 degrees C. This is inconsistent with our lead free solder profiles which require a nominal 245 degrees C.
We noticed the TL4051 has the same package and pin out, but there is no specification of the max. reflow temperature in the data sheet. Could you please provide this information? Thanks and Best Regards,
-Tim Starr on behalf of TI@LT