TPS62290 for Sartan VI FPGA
One of my customers wants to use TPS62290 to get 2.5V & 1.0 to his Spartan VI FPGA. His input is 4V, out put is 1V@1A. When he uses Switcher Pro, the software suggests to use 10uF cap. However, his load is 470uF, so he changes to that. The phase margin decreases by 30 degrees or so. His question is, would this cause any problem or not. regards