Hi,
I have a fuel gauge in a battery pack, and have noticed that during discharge the NAC (nominal available capacity) decreases gradually from the starting value of about 1500mAh until it reaches 560.13 mAh, and then it stops updating. However, the voltage is still at 3.3V, and the current draw is 7443mA.
As well, when the reported voltage drops below 3.4V, I am not seeing the EDV1 flag go high to indicate that the battery is getting low.
A few observations:
1) the reported temperature has just reached 40 degrees C when the NAC freezing occurs
2) the pack fuel gauge sense resistor is two 20mOhm resistors in parallel, and the current draw is 7.4A, so we have a voltage of 74mV across SRP and SRN
3) During charge of the pack
- we are charging the battery to 4.2V, but the charge termination is set to 4.112V.
- our battery charge circuit cuts off the current to the battery when the taper current has dropped to 150mA, but the TAPER current is set to 91mA (I will increase this in the EEPROM)
Anyone have any ideas about what I'm doing wrong?
Thanks,
Alex