My input voltage is 7.4 volt and required voltage is 12 v....but 12volt required for initially to boost system...the system will take load current around 3-4A.
suggest boost converter...
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
My input voltage is 7.4 volt and required voltage is 12 v....but 12volt required for initially to boost system...the system will take load current around 3-4A.
suggest boost converter...
Milind,
What is the input voltage range? Is Vin=7.4V the minimum input voltage? and the output is setting at 12V/4A. If it is so, TPS61088 is just fit for your application. You can apply for a TPS61088 EVM board to test the performance by contacting the local TI FAE.
BR, Helen