Hi everybody,
is it possible to wire some parallel DSG-FETs in parallel to one CHG-FET? I want to do that because the discharge current is approx. 10 times higher than the charge current and the CHG-FET dont has to conduct all the discharge current.
Otherwise (DSG and CHG FETs serial) I have to use the same number for CHG-FETs.
Are there some special problems with the bq79640 I cant see?
Thanks a lot
Armin Nestler