Hi, my design spec is 6W, 15Vin -> 2 separately isolated 15V outputs with reasonably loose regulation requirements i.e. +-0.5V would be fine.
Output 1 - 15V, 300mA
Output 2 - 15V, 100mA
Isolation pri->sec 4kV, sec->sec 4kV
I'm thinking this could be a candidate for PSR flyback to achieve a cheap design, given that output 2 is lightly loaded and will stop conducting long before output 1.
Reading the datasheet for UCC28911 (figure 48) it seems that some implementations of PSR would handle this pretty well.
Can anyone shed any light on whether this would be a good idea, and whether there is a integrated switch IC more appropriate to the voltage/power level that would work doing PSR in this situation?
http://www.ti.com/product/UCC28911/datasheet/applications_and_implementation
Thanks