i am a student and beginner with battery management i have bq40z60 evm board from ti and ev2400 interface board . i installed bq studio v 1.3.47 on windows 10 pc and updated ev2400 firmware .now when i connect ev2400 with pc and bq40z60 with ev2400 using SMB port 1 , bq studio does not auto detect the device and in manual it shows two bq40z60
4600_0_13_bq40z60.bqz
4600_0_15_bq40z60.bqz
which one i use to connect .
- where I learn about the control of charging ,balancing,measure soc ,discharge control using bq40z60 and bqstudio.i have li ion cells and want to make a battery pack using bq40z60.
thanks
vijay singh
vijay.kajla.in@ieee.org
India