Hi,
I've recently rebuilt a design and ironed out what I hope is the majority of the operational issue. Now I'm just working on operating within the correct margins, but I'm seeing a few issues here and there.
Firstly, I change the Rlim resistor to avoid damaging any of the other components, which had happened previously. I wanted to limit the current at about 4.2A, therefore selected a resistor of 0R06 (I'lim = 0.254 / R'lim).
However, what I am noticing is that I am only ever seeing a peak current of 2.8A, where I'd expect it to be >3.5A. I realise it may not be Rlim that is causing this, which is why I've come here to ask. What else might be causing this lower than expected output? Could it be due to the analogue dimming set up?
Secondly, I am having a little trouble with my UVLO hysteresis. As per other advice received on the forums I inserted a series resistor between the voltage divider since I was seeing a sizeable ringing on the nDim pin and was concerned it might cause issues as the cut off approached. What I'm seeing now is, even though (i think) my divider is set to cut off at 6.5V, Vin can go all the way down to about 5.4V before it cuts off. A less important point to note is that as it approaches this threshold the brightness of the LED increases if it's not set to maximum brightness.
I also notice that the LED brightness seems to increase slightly with the voltage input from about 6.5-9Vin. When it reaches the 9V mark it sort of snaps back into being a stable output again. Can this be resolved?
Thoughts on any of this?