Hi,We are planning to use TPS92314A LED driver IC for driver applications upto 80Watts. we have made pilot assemblies for 50W drivers(60Vx0.75A) for universal input range from 85V to 300V AC.The transformer and the circuit components have been calculated using the relevant TI design tool. The Driver starts working only around 160V AC input. The start up resistor was reduced to 100K.ohm and the Bias cap used is 10Mfd/50v elco. The LEDs start blinking at about 90volts and fully turn on at 160Volts. The comp.cap is 4.7mfd and the ZCD resistor divider is 68K and 12K. The input tank cap is 0.22mfd/630V
Once the LEDs light up the input voltage can be taken down to as low as 70Volts AC and LEDs remain lit. At 230V AC the output current is 750mA @59.5V. And the efficiency is 88% THD is 15% and input PF is 0.95. The Aux supplied Vcc is 20Volts.
The transformer is sandwich wound and the winding sequence is as follows: Half primary first, Aux next,secondary next and balance Half primary last. We interchanged the positions of Aux and secondary windings with no change in results The ZCD wave form on the IC pin is 3 Volts peak to peak.
Please advise how to get the driver to start working around 85V AC input? Look forward to an early response.
S.Ramakrishnan