BQ40Z60
My original design calls for a +21V DC external DC supply to drive the VAC (Charger Voltage) inputs. According to the reference design, the return terminal is connected to PACK GND rather than system GND.
The design has changed as we are now using a TI TPS61175 Boost Converter (from +12VDC to +21VDC). Is it still necessary to connect the boost converter ground returns to PACK GND?
Note: I've retained a VAC snubber circuit to avoid damaging the TPS61175, as was done in the prior design. However, I'm tempted to connect the snubber ground return to system GND. Would rather have a current spike on that bus instead of PACK GND... but perhaps this is also not wise?