1) The RT pin is tied to VREF (61.9kohm) which configures the part as a master but the SS/EE pin has a 825kohm resistor to GND for a slave configuration. What does this combination master/slave accomplish vs. removing the 825kohm resistor?
2) Equations 10 and 11 in the Rev C datasheet compute Fsw vs. RT for master and slave configuration then has a comment that the equations are equal when VREF=5V. The reference is fixed so when would these be different?