This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq27542-G1 - Hardware config of TS pin when external thermistor unused

Other Parts Discussed in Thread: BQ27542-G1

Hello,

If the external thermistor feature of bq27542-G1 is not being used (set to read from the internal temp sensor instead), how should the TS pin be treated?

I've seen recommendations to pull TS to VSS with a 10 kohm resistor for other gauges, but it doesn't explicitly say in the datasheet or TRM (that I could find).

Thanks,

Jonathan