Hi,
I am looking for this kind of solution:
- Input – 9-16VDC
- Output – Dual , ±6VDC, 2-3A.
I believe TPS54340 can be a good solution.
Any ideas?
Thanks in advanced.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
For the inverting buck-boost, the current is derated by a factor of 1-D. You could theoretically use a split rail supply as shown here with the TPS54340:
But you will get less than 3 A total for both rails. Alternately you could use two TPS5430, one as a standard buck to get +6 V at 3 A and another in inverting buck-bost to get -6 V at close to 2 A.