For the MC33063ADR, we have a lot more questions. We want a Vout of 9V, so based on the equation provided R2/R1 = 6.2. However, we were not sure what range of values to use. Going off of the application schematic, we were assuming between 2-100k ranges. Based off of that, an early guess would be R1= 2.2 kΩ and R2=13.6 kΩ. Another issue was how to properly to determine Vf and Vsat. Lastly, we weren’t sure what would be good values for the minimum switching frequency or the ripple voltage. Obviously, the ripple should ideally be low so we must use a bigger capacitor for Co. However, Ct, Lmin, and ton are all dependent on the switching frequency and their function in the circuit is harder to predict, making it harder to choose values for them. Lastly, we wanted to check the purpose of the optional LC filter; we are not sure if it is present to further reduce ripple and noise or if it serves any other purpose.