This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3480 capacitor stability

Other Parts Discussed in Thread: LM3480

Hey team,

I am looking at this LDO LM3480 on ti.com.

Is this stable with both ceramic and electrolytic capacitor at the input and output terminals?

I tried to look for this information in data sheet but could not find it.

 

Thanks,

Yiding 

  • Yes.

    A point on the electrolytic capacitor ESR at the output terminal to keep in mind:

    If the application load is prone to abrupt changes in load current (i.e. fast edged load steps) the ESR in the electrolytic capacitor may cause undesirable voltage spikes. This is not a fault of the LM3480, it's just how high ESR capacitors behave with fast load steps.

    See Application Report SLVA072, Section 7,Transient Response:

    www.ti.com/.../slva072.pdf

    If load current is quiet and steady, then no worries.