This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54620 parallel operation

Other Parts Discussed in Thread: TPS54620

Hi,

I have connected two TPS54620 buck converters in parallel operation, I have followed the schematic diagram of the parallel operation in the product folder. However, when I increase the output load current, one of the buck converter output current will increase and the other one will decrease and become negative, can anyone help to see why like this? By the way, the output voltage is very stable which is 5V. 

Thank you.