This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

The LED of STAT1 of the BQ24104 is blining

Other Parts Discussed in Thread: BQ24104

Hi,

I use BQ24104 to charge the 3.7v 6600mAH 18650 package, the designing charger current is 1.6A(actually 1.5A), the charging termination current is 0.445A(actually 0.387A).

During the charging process, when I the charging time is about 4 hour and a half hour,  the LED of STAT1 of  the BQ24104 start blining.  It make no effect when I pull out battery,  disconnect the adapter. Below is my sch.

It blining with the frequecy of 0.5Hz, and i check it in the datasheet.

When it start blining, i measure the battery voltage, and it is 4.04V. And the temperature is around 20 degree. I set the fast charge time as around 9 hours through C8. So it seem the problem is no the same as what the datasheet describes.

But i found a phenomenon that when i change another battery(voltage is around 3.9V), it become nomal. But when i insert the battery i say before, i blining again!

So, what's the reason? Can anyone help me?

Wish for anyone's reply. Thanks