This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Bq34z100-g1 Lead Acid 12v 7200mA/20H

Other Parts Discussed in Thread: BQ34Z100-G1, BQ34Z100

Dear Sirs;

I have no experience with Gauge bq34z100-g1 and I need help to program it and put it to run.
My battery is lead acid 12V 7A / 20H, MODEL 6FM7 NLD POWER, www.indpower.com.
The resistive divider to the ci bq34z100-g1 pin 4 is 253K and 16K5 and the shunt resistor used is 100m Ohm. The resistive divider this directly connected to the battery without control pin 2, VEN.

I will not use LEDs, communication with the microcontroller is just the I2C signals SDA and SCL.
Can You send a procedure for programming this registers step-by-step, with all values values ?
This procedure must enter all necessary actions to set the Gauge bq34z100, step by step.

Sure your attention, thank you in advance.

Best regards;

Adilson Medeiros

  • Adilson
    I do not have a document that provides a step-by-step procedure to configure every parameter in the gauge. The closest that I have to offer are sections 9.2.2 and 9.2.3 of the datasheet. You can use these sections and let me know if you have specific questions. You can export and attach an srec file after you are finished and I can help to review it.

    Tom