Using TPS7A8300 in "any-out" config. Vin=3.1V, Vout~3V (programmed to 2.8V), load current=500 mA, external on/off control using EN pin.
Output sits at about 3V, but it is programmed to 2.8V. If I touch some of the pins, I can move this voltage around by a few 10s of millivolts - does not seem stable.
We have a few of these chips in our system. Some operate fine, while others don't seem to regulate. The ones that are not regulating also do not have any control on output voltage if I change state of programming pins.
Cin= 10uF(ceramic), Cout=30uF(ceramic)