This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2060CDGNR / TPS2066CDGNR Thermal Information

Hi,

Please help to confirm below parameters of TPS2060CDGNR / TPS2066CDGNR.

It don't be mentioned in the datasheet.

Thank you very much!

Supplier

 

Supplier P/N

 

Peak Temperature

(TC)

Thermal Spike

 

Preheat Temperature

(Maximum Time)

Time Above 217°C Liqudous

Temperature (TAL)

Ramp-down Rate (°C/S)

 

TI

TPS2060CDGNR

 

 

 

 

 

TI

TPS2066CDGNR

  • Hi again, Daniel.

    I am not sure the requested information is available but I will check internally. Within the datasheet, there is the packaging information on page 24 which has MSL Peak Temperature and operating temperature. Towards the front of the datasheet, there are absolute and recommended temperatures.

    Can you tell me why this information is needed? Is it for a soldering temperature profile? If so, we leave that up to the individual customer's manufacturing needs and requirements as these package types are quite common.

  • Dear Eric,

    Thanks for your support. This question is from my customer's server project. I am not sure about the exact reason for the request. My customer will set a parameter database for application.
    Please reply it as soon as you get the data from thermal modeling team, this case is a little urgent from customer.

    Thanks
    Daniel

    daniel.chung@wpi-group.com