I am using the BQ24620 to power a 4 cell battery pack based load. (upto 14.4v). However, I would like the unit to be powered up at a constant voltage even the battery is not detected.(Battery is optional for this application)
Is it possible to modify the circuit to allow this? So far, the way to do this is exceeding CMAX on the load (Equation 8 on page 22 of the datasheet) This comes out to be around 700uF for my circuit. Is there any other way?