This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Using the BQ2000 in a standby mode

Other Parts Discussed in Thread: BQ2000, LM3671

I have a situation where I use a 12V wall-wart to power two parallel circuits. The first is a switcher that brings the voltage down to 8V. The second uses the 12V to power a BQ2000 that's set up to charge 4 NiMH cells. Each of these is diode OR'ed to generate a power bus. The intent of the design was that when AC is present, the wall-wart would drive the bus to 8V. When the AC failed, the NiMH cells would drive the bus at 4 to 5 V.

However, what I'm seeing is that when the AC is present, the pulses out of the BQ2000 circuit go up the 12V level and momentarily drive the bus that high. Is this the nature of the BQ2000?

In order to do what I want, should the BQ2000 draw its power from the 8V bus? This would prevent any spikes that are higher than the existing bus but would require more current through that circuit.

Note: A full circuit can be posted if that would help.