I am facing a problem with two pins 2&3 and 10&11. should I leave one pin of each unconnected or short it together? please help me.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am facing a problem with two pins 2&3 and 10&11. should I leave one pin of each unconnected or short it together? please help me.
Please refer to the schematic in the users guide. Pin 2 and 3 should be shorted and pin 10 and 11 should be shorted. BAT and OUT can be high current path, thus by shorting two pins, it increase the width of the current path and will result in better thermal performance.