Hi everyone,
We are currently developing a project in which we would love to use BQ24030 due tu its features as SAI, automatically selectable AC / USB power inputs, AC power input range up to 18V, etc.
The fact is, we do need some more features the BQ2040 does not have, as the following ones:
- When sourcing power from battery, desirable Vout=5V, rather than Vbat (it is needed an internat boost).
- Iout = 3A (or more), regardless of sourcing from AC / USB / BAT rather than 1,5 when sourcing from BAT.
The question is: Is there a newer version of this IC that would perform the old features and the new ones we need?
Thank you in advance!