Hi there,
I am working on a basic constant current source 3.7 V Li-Io battery charger. It consists of the LM317, a NPN transistor, some resistors, and capacitors. I set the open circuit voltage difference to be 4.1. However, when I connect the battery in I get no extra current draw compared to the 1mA the chip using while under no load. While testing in simulation, the circuit was able to draw the desired 700 mA to the battery. I have attatched in a word document showing my working circuit in LTSpice and my implemented circuit to get the 4.1 voltage difference. Please let me know your thoughts.
Thanks,
David MunzerBattery Charger Schematics.docx