I am using the REG104-A to power a small incandescent lamp (2.9V @ 700mA). Because a cold lamp filament presents a very low resistance, the current surge as the lamp turns on can be rather high. The REG104 will current limit this to1.7A (typical), which is actually desirable, but I noticed that as the input/output differential falls below ~0.7V , the current limit rises suddenly to about 2 Amps. At this point the lamp reaches operating voltage and its current draw falls as its impedance rises.
There is nothing in the datasheet to suggest that the current limit of this device depends somewhat on input/output differential. Is there any additional data available or does anyone have any experience with this? I would like to know what the limits on this behavior are and what it does over temperature.
Thanks
~Tim