Using TPS61199 to drive two LED strings. One string with shunt protectors. The other one not.
IFB1-4 to drive one string and IFB5-8 to drive the second one. TPS61199EVM-598 is used with default settings. So each string sees ~240mA current.
Here are the waveform on the IFB pins. Ch2 is the string with shunt protectors. One LED was taken out to see the protector active working. The voltage settling time is quite long (~10us). And the TPS61199 device seems not liking it and turn these channels off after one or two seconds (See second picture)
Tried to put a 33nF cap on the IFB pins to ground. Still did not work although the surge was damped.
Any suggestions are greatly appreciated.